Solution


Wireline Pump Down

Pump down operation is used for horizontal wells in the oil field. Fluid is pumped to push tools down deviated or horizontal wells.


WirelinePumpdownGraphic Color

Summary

  • Customer Need / Challenge

    Pump down operation is used for horizontal wells in the oil field. Fluid is pumped to push tools down deviated or horizontal wells. Operations could include plug setting, and perforation. Accurate tool string tension readings are required for this downhole procedure.

  • Interface Solution

    The IPCD Pressure Compensated Downhole Load Cell is an accurate and superior load cell over wet or hydraulically compensated load cell options. Featuring proprietary pressure and temperature compensation, offering precise and real-time tool string force measurements.

  • Results

    Customer was able to carefully regulate tension forces on the toolstring during the pump down procedure, avoiding expensive pump off tool separation.

Materials


  • IPCD Pressure Compensated Downhole Load Cell
  • Customer Instrumentation

How it Works


  1. The IPCD Pressure Compensated Downhole Load Cell is attached at the top of the tool string.
  2. During pump down, the IPCD measures the tension between the cable head and the tool string.
  3. Connected to the customer’s instrumentation, actual cable head tension is closely monitored during the pumpdown process.

Download PDF